Indian Navy Dredger: Completes Successful First Year | Cummins Inc.
""
Marine

Indian Navy Dredger: Completes Successful First Year

by Alan Haig-Brown

Cummins Vessel Reference 784

 

In mid-April of 2016, the Indian Navy’s grab hopper dredger, Dredger-1 was preparing to depart its birth shipyard following a comprehensive one-year warrantee review. Tebma Shipyards Ltd., Senior Vice President M. Balasubramaniam explained that the 44.15 by 12.2-meter vessel was designed to meet precise deepening requirements around docks and port installations and in riverine or other places where deepening of specific areas is required. The vessel has a 320-HP Cummins-855-powered forward-mounted crane supplied by Titagarth Wagons. The crane’s 15.2-meter boom has a working radius of 12 meters and hoisting capacity of 10.5 tonnes at a 46-degree boom angle. The crane’s grab bucket has a 3-cubic meter capacity to hold 4.5 tonnes of dredge materials. The crane is capable of dredging up to a depth of ten meters.

 

The crane transfers the dredged material to the ship’s hopper which is of 300 cubic meter capacity, (500 tonnes). The dredged material in the hopper is dumped at the open sea through a set of eight hopper doors controlled by hydraulic rams and chains over pulleys. The main propulsion for the dredger is a pair of Cummins KTA38-M engines each producing 1000 HP at 1800 RPM. These engines are built in India and meet the Indian Navy’s policy of supporting domestic suppliers. Cummins India Ltd. (CIL) was set up in Pune in 1962. Today, CIL is India’s leading manufacturer of diesel engines with a range from 15 kVA to 2000 kVA and value packages serving the Power Generation, Industrial and Automotive Markets. CIL’s products include diesel and natural gas engines in the range of 65 HP to 3,500 HP. It manufactures over 35,000 engines and gensets per annum and is among India’s largest exporters of engineering products.

With the one-year warrantee review completed, the Dredger-1, has left the Tebma Shipyard and will resume duties with the Indian Navy at Naval Dockyard, Mumbai.

 

Photo courtesy of Tebma Shipyards.

 

For further information:

 

M. Balasubramaniam
Senior Vice President (SB-C)
Tebma Shipyards Ltd.
11 Floor, MT Rajen’s Properties
40, Bazulla Road
T Nagar, Chennai, 600 017
Phone: +91 44 2834 9415
Mobile: +91 98400 71760
E-mail: [email protected]

 

Rajesh K Yadav
Senior Manager -Marketing & Sales (Marine)
Industrial Engine Business Unit
Cummins India
India Office Campus, Survey No.21
Balewadi, Pune – 411045
Phone: +91 20-67068715
Fax: +91 20 2538 1591
Mobile: +91 735001 1959
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...