Make Over for Landing Craft | Cummins Inc.
""
Marine

Make Over for Landing Craft

by Alan Haig-Brown

Cummins Vessel Reference #632

At the launching in Vietnam.

The iconic 4-wheel-drive World War II Jeep has undergone decades of upgrades to become the modern SUV. Now the craft that landed on the beaches of Normandy and the islands of the Pacific has been similarly upgraded at the South East Asia Shipyard in Vietnam.

With ro-ro containers.

The most important factor in the design, by France’s Piriou Ingénierie, is the provision for the landing craft to carry up to nine TEU of containers on trailers as well as regular cargos. Side rails will secure the trailers and their containers. Electric connections will be provided for reefer containers. The trailers and other cargo will be loaded and off loaded through the hydraulic controlled forward cargo ramp.

The advent of containerized shipping has put many small island and coastal communities at a disadvantage in shipping products such as locally caught fish. There has also been difficulties in the importation of containerized consumer goods. The 39.8 by 9.8-metre landing craft will be put in service between St Martin and St Barthelemy Islands in the West Indies. The vessel, owned by RMP Caraïbes, is surveyed by BV and will be French flagged.

To be named Hirundo, Latin for swallow, the vessel is powered by a pair of six-cylinder Cummins KTA19 engines each rated for 425 HP at 1800 RPM. These engines will turn fixed pitch four-blade propellers through ZF360 gears with 2.917:1 rations. Two Cummins powered Leroy Somer generators with outputs of 106 KVA and 65 KVA will provide electrical power. Both generators are 50Hz and 230-400 V tri-phase systems.

Fuel and water capacities are 34 cubic meters and 7.5 m3 respectively. To be operated by a crew of four, the boat will be delivered to her owners via a heavy lift ship from Ho Chi Minh City to Pointe a Pitre, Guadeloupe and then on her own keel to St Barthelemy. This revision and update of the classic landing craft offers potential for many areas worldwide that are too small for a conventional container port.

Illustration and photo courtesy of South East Asia Shipyard

For further information:

Damien Gay
South East Asia Shipyard
Ap Thuan Dao, Thi Tran Ben Luc,
Huyen Ben Luc, Tinh Long An,
Vietnam
Phone: 84 723 63 5294
Fax: 84 723 63 5294
E-mail: [email protected]
Web: www.piriou.fr/en/the-sites/seas/36.htm

RMP Caraïbes
Quartier de Public, 97133 Saint Barthélemy
Phone: 590 27 9800
Fax: 590 27 6281
Web: www.rmp-caraibes.com/

Tommy Quan
Area Manager
South East Asia and Korea
Singapore
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...