Argentina Continues to Build Fleet | Cummins Inc.
""
Marine

Argentina Continues to Build Fleet

by Alan Haig-Brown

Cummins Vessel Reference #654

 

The Argentine shipyard Astillero Naval Federico Contessi Y Cia SA has been busy with fishing boat orders. In March they launched another of their fine new trawlers. Amid much fan fare, fire works and confetti the B/P Nono Pascual slid down the ways. On hitting the water, her 600 HP Cummins KTA19 M3 was started and the boat made a celebratory lap of the harbor to the continuing cheers of the shipyard crew and invited guests. The owner, Canal De Beachle SRL, will put the vessel right to work and can expect many thousands of hours of service from the boat and its engine. The six-cylinder in line KTA19 has proven itself time in terms of cost to operate and time to over haul in fishing fleets from the Bering Sea to the South China Sea and from the North Atlantic EU states to the South Atlantic waters where this new boat will be working.

 

 

 

 

The KTA19 rated for 600 HP at 1800 RPM turns a 1750 mm propeller in a nozzle through a Twin Disc MG 5222 gear with a 6:1 ratio for speeds just under ten knots. The 25.2 meter by 7-meter boat was designed by Marine Engineer Angel S. Coronel. It has a 40 ton hold capacity and accommodation for a crew of up to ten fishermen.

 

Fuel capacity is 35,300 liters an water is 25,500 liters in the hull which has a depth of 3.2 meters. Auxiliaries for powering generators and auxiliary hydraulics include two Cummins 6 CTA8.3 G engines. Some onboard processing of the catch can be undertaken in the covered deck area.

Engine room gauges showing RPM and Exhaust temperature.

 

The Nono Pascual is the owners, Canal De Beachle SRL’s, third vessel. The family owned company now has three Cummins powered vessels. The Jupiter II is powered by a Cummins KTA38 M0 while the Canal de Beagle is, like the Nono Pascual, powered by a KTA 19 M3. In addition to their three boat fishing fleet the company also has a shore side facility where they process anchovies for export to Europe and other species.

 

 

For further information:

 

ASTILLERO NAVAL FEDERICO CONTESSI Y CIA SA
Calle “B” Espigón 4 Puerto – (B 7603BHP)
Mar del Plata – REPUBLICA ARGENTINA,
Phone: 54 0223 489 0314

Angel S. Coronel
Marine Engineer
Lebenshon 2767 (7600)
Mar del Plata
Phone: 54 0223 480 0550

Armando Tavarozzi
Marine Engine Sales and Application Engineer
Cummins Argentina
Phone: 54 11 4736 6428
Fax: 54 11 4736 6466
Cell: 549113280 8713
 

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...