Case Studies | Cummins Inc.

Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Cummins Vessel Reference #806       Rendering of the port bow quarter showing pin location in raised forecastle.     Vancouver, BC based Island Tug and Barge has a reputation for excellence in their vessels and equipment. Over the years they have refurbished and repowered older vessels and completed new vessels. They are currently working on their mo

Cummins Vessel Reference 1. The PAP Moralesm’s fine hull shape is evident in this image from the launching.   The Peruvian Navy has recently taken delivery of a well-equipped dive support vessel (DSV) from the shipyard Servicios Industriales de la Marina S.A. (SIMA). Designed in-house by the shipyard, the new 4400 HP vessel has significant towing capabilities and can act as a sal

Cummins Vessel Reference #804 Water taxi: 12 by 2.5-meter powered by Cummins 6BTA-M 5.9-liter.   For many years, the Supatra River House on the Chao Phrya River, has been a favorite with Thai and foreign dinners. Situated on the Thonburi side of the river, the most favored approach to the restaurant is by boat. To that end, the owner, Khun Supapan maintains a fleet of beautifully

Cummins Vessel Reference #803 Boat is 22 X 6.5 meters, with new 4BTA3.9 GM-Cummins genset, for extensive electrical needs in galley   Visitors to Thailand, like the Thai people themselves, invariably comment on the diversity and complexity of Thai food. It is the result of many centuries of refinement and a dedication to fresh ingredients. From the beach restaurants of Phuket to

Series II Birdon Bridge Erection Boat The US Army Bridge Erection Boat.   Quick assembly floating bridges have been a military standby for the US Army since, at least, World War II. Improvements over the years have allowed for ease of transportation and rapid deployment. In the early 1980s, specially designed Bridge Erection Boats (BEB) were developed. They could be transported b

Cummins Vessel Reference #810 A state-of-the-art dive-support vessel is a marvel of modern technology and design. Seldom has this been more evident than in the Oceanicasub V, delivered in February 2017 to her Brazilian owner Oceânica. Oceânica provides subsea services to the petroleum company Petrobras. The Oceanicasub V is the second in a pair delivered from the Arpoador Shipyard in Gua

Cummins Vessel Reference #776 The M/V Tom Cotton ready for work. Blessey Marine has a long history of growing one of the largest fleets of towboats and petroleum barges on American inland waterways. The majority of barges are 10, 20 and 30 thousand-barrel clean/chemical barges and 30,000 black oil/asphalt barges. In addition, the company has a number of stainless and pressure barges. To push th

Cummins Vessel Reference #802 Jensen Design and Rendering   Shipyards, especially those that repair and construct larger vessels, invariably need to move the vessels, materials and other resources about the yard. To do this, yards often have a small yard-tug that can maneuver in and around yard structures such as for repositioning bulls into dry docks or to control newly launched

Cummins Vessel Reference #797 53×26’6x14-foot draft, 2X KTA38-M2 1200 HP each at 1800 RPM AG McIlwain design   Steady, smooth, powerful, highly maneuverable,” these were comments by mariners, who were onboard for sea trials of Jones Marine Group’s new tractor tug David J. The new boat was put through its paces in fine form. The boat is an A.G. McIlwain-designed 53 by 26.5-foot h

Cummins Vessel Reference #799 Built Nichols Bros to Jensen design, the Oscar B departs the Oregon shore. Since 1925 there has been some form of car ferry crossing of the lower Columbia River from Puget Island on the Washington side to Westport Slough on the Oregon side. In 1959 Wahkiakum County took over operation of the ferry and in 1962 had a steel-hulled ferry, named for the county, built by

Cummins Vessel Reference #798   When Gustavo Galeano first started up the engine after his new boat, Don Franco, was launched in the spring of 2015 he was greeted by a familiar sound. The solid throbbing of the 600-HP, Cummins KTA19 main engine reminded him of the Cummins engine in his father’s boat. The connection over generations is of great importance to commercial fishermen who

Cummins Vessel Reference #789     The Brutus alongside for commissioning ceremonies.   In May of 2016 the Argentinian-designed and built 28.77 by 10.2-meter ASD tug Brutus went to work in the Harbor at Buenos Aries. This marked a milestone in Argentinian maritime affairs, as it is, at 5,400 HP, the most powerful ship-handling tug in the country.  

Cummins Vessel Reference #796 An outboard profile for the three Cummins-powered ATB building for Vane Bros. The bold blue “V” logo emblazoned on the green-banded white stack continues to proliferate on American waterways. Vane Brothers Company has been expanding its fleet with new construction. Recently the marine transportation company announced a contract for three ATB tugs to be built at the

Cummins Vessel Reference #795 A rendering of the Global Provider to by launched in early 2017.   We wanted a vessel that would allow us to quickly and efficiently serve our diesel and lube oil customers in Puget Sound” explained Maxum Petroleum’s Mike Curry of the new 126-foot product tanker that the firm is having built. “We have 15,000 barrel barge doing the job now but this bo

Cummins Vessel Reference #790 The TG17 rendering shows a good looking and versatile boat.   A challenge for designers or an emergency response vessel is deciding to what type of emergency the boat will respond. The designers at the non-government Marine Engineering Bureau in Odessa Ukraine have fitted a very wide range of capabilities into their 31.73 by 9.7-meter tug. The vessel

Cummins Vessel Reference #788 Vietnam, with a coastline of 3,260 kilometers, excluding islands, claims 12 nautical miles as the limit of its territorial waters, an additional 12 nautical miles as a contiguous security zone and 200 miles as an exclusive economic zone. This adds up to a lot of water to protect as well as a rich coastal fishing area.   Bui Mong on his new boat.

Cummins Vessel Reference #787 Built Goa Shipyard, Vasco, Goa, 14.3 X 4.0 X .9 meters, 2 x QSC 8.3 500 HP, ZF 286 gear, RR jets, 35 knots, delivered Jan 2016   Mauritius is an island nation in the southwestern Indian Ocean. The country has just 2,040 square kilometers of land on several islands but a huge exclusive economic zone (EEZ) of 2.3 million square kilometers. The major ch

Cummins Vessel Reference #786 Still in the river, the new boat looks anxious to get out to sea to show her stuff.   There is something about Italian products, from consumer goods to industrial objects, that carries a stylistic flair. This is well represented in the cruise ships of the Fincantieri Shipyard, such as the 2015-delivered Britannia. More recently this flair for design