ELIMINATOR | Cummins Inc.

cummins eliminator placement illustrationAvailable on the KTA38, KTA50, and all QSK MCRS engines, ELIMINATOR is a combination full-flow and centrifugal system that incorporates a permanent stainless steel core that eliminates the need for disposable oil filters.

ELIMINATOR (outlined in red in the photo) consists of a two-stage filter media system. The first filter screens for particles as small as 20 microns, while a centrifugal separator constantly spins, depositing the heaviest particles on a replaceable liner.

Because ELIMINATOR uses the oil pressure in the lubricating system to spin the centrifugal separator, there is no additional load on the engine, with no drain on power or fuel economy. This option lowers the cost of operation by:

  • Eliminating the recurring cost and maintenance of spin-on filters
  • Reducing downtime for filter changes
  • Eliminating disposal cost of used filter elements
  • Improving filtration and reducing component wear which can extend overhaul periods
  • Extending oil change intervals when used concurrently with oil sampling and CENTINEL

ELIMINATOR satisfies most Marine Classification Society requirements for duplex filters.

Case Study Actions

Versatile Harbour Tug with Cummins QSK60

View

Sophisticated New Trawler from Danish Yard

View

Tom Aliotti: Designed and Built by Fishermen for Fishermen

View

Bristol Bay: Everything in 32 Feet

View

Launching A Traditional Ship with a Contemporary Heart

View

State-of-the-art dive-support vessel is a marvel of modern technology and design

View

Tug: 3200-HP Ready to Work

View

ASD New Build from Vitawani

View

Catamaran-Mounted Remote Controlled Net Cleaner

View

Articulated Tug & Barge (ATB) for Island Tug & Barge (ITB)

View


To view all case studies, click here.