ELIMINATOR | Cummins Inc.

cummins eliminator placement illustrationAvailable on the KTA38, KTA50, and all QSK MCRS engines, ELIMINATOR is a combination full-flow and centrifugal system that incorporates a permanent stainless steel core that eliminates the need for disposable oil filters.

ELIMINATOR (outlined in red in the photo) consists of a two-stage filter media system. The first filter screens for particles as small as 20 microns, while a centrifugal separator constantly spins, depositing the heaviest particles on a replaceable liner.

Because ELIMINATOR uses the oil pressure in the lubricating system to spin the centrifugal separator, there is no additional load on the engine, with no drain on power or fuel economy. This option lowers the cost of operation by:

  • Eliminating the recurring cost and maintenance of spin-on filters
  • Reducing downtime for filter changes
  • Eliminating disposal cost of used filter elements
  • Improving filtration and reducing component wear which can extend overhaul periods
  • Extending oil change intervals when used concurrently with oil sampling and CENTINEL

ELIMINATOR satisfies most Marine Classification Society requirements for duplex filters.

Case Study Actions

Higman Marine Selects Electronic Tier 3 Cummins

View

Indian Navy Dredger: Completes Successful First Year

View

Malaysian-Built Fisheries Research Vessel for Bangladesh

View

Rodriguez Tow Boat For Mid-River

View

Versatile Tug for Port of Toronto

View

Willard Marine’s Twin Diesel RIB

View

Seaspan Venture: Like for Like

View

Vietnam Grows the Fleet

View

And So the Fleet Grows

View

Seacor Marine’s 13,400 HP Vessel Delivered

View


To view all case studies, click here.