ELIMINATOR | Cummins Inc.

cummins eliminator placement illustrationAvailable on the KTA38, KTA50, and all QSK MCRS engines, ELIMINATOR is a combination full-flow and centrifugal system that incorporates a permanent stainless steel core that eliminates the need for disposable oil filters.

ELIMINATOR (outlined in red in the photo) consists of a two-stage filter media system. The first filter screens for particles as small as 20 microns, while a centrifugal separator constantly spins, depositing the heaviest particles on a replaceable liner.

Because ELIMINATOR uses the oil pressure in the lubricating system to spin the centrifugal separator, there is no additional load on the engine, with no drain on power or fuel economy. This option lowers the cost of operation by:

  • Eliminating the recurring cost and maintenance of spin-on filters
  • Reducing downtime for filter changes
  • Eliminating disposal cost of used filter elements
  • Improving filtration and reducing component wear which can extend overhaul periods
  • Extending oil change intervals when used concurrently with oil sampling and CENTINEL

ELIMINATOR satisfies most Marine Classification Society requirements for duplex filters.

Case Study Actions

Combination Tug & Dive Support for Peruvian Navy

View

Chao Phraya: A Floating Food World

View

Teak Dinner Cruise: For The Chao Phraya River

View

Purpose-Built Yard Tug

View

Speed, Innovation, Luxury, Fun

View

Shallow-Draft Yukon River Tender

View

Oscar B: Power in the River Currants

View

Reliability, Good Power, Low Fuel Consumption

View

Handy Size, Ample Power, Ship Handler

View

Powerful New ATBs for Vane Bunkering

View


To view all case studies, click here.