ELIMINATOR | Cummins Inc.

cummins eliminator placement illustrationAvailable on the KTA38, KTA50, and all QSK MCRS engines, ELIMINATOR is a combination full-flow and centrifugal system that incorporates a permanent stainless steel core that eliminates the need for disposable oil filters.

ELIMINATOR (outlined in red in the photo) consists of a two-stage filter media system. The first filter screens for particles as small as 20 microns, while a centrifugal separator constantly spins, depositing the heaviest particles on a replaceable liner.

Because ELIMINATOR uses the oil pressure in the lubricating system to spin the centrifugal separator, there is no additional load on the engine, with no drain on power or fuel economy. This option lowers the cost of operation by:

  • Eliminating the recurring cost and maintenance of spin-on filters
  • Reducing downtime for filter changes
  • Eliminating disposal cost of used filter elements
  • Improving filtration and reducing component wear which can extend overhaul periods
  • Extending oil change intervals when used concurrently with oil sampling and CENTINEL

ELIMINATOR satisfies most Marine Classification Society requirements for duplex filters.

Case Study Actions

Pocket Tanker for Puget Sound

View

Aitana B: Power and Versatility

View

Big Hours, Little Wear

View

Revisiting The US Army’s Bridge Erection Boat

View

World’s Leading Manufactures for Russian Tug

View

Versatile Response Vessel from Russia

View

Argentinian Brutus At Work

View

Vietnamese Fisherman Opts for Cummins and Fiberglass

View

Small Nation, Big Marine Territory

View

Italian Crewboat: Excellence in Design, Quality in Construction

View


To view all case studies, click here.